Reply
Highlighted
Avnet Employee (Regular Contributor)
Posts: 24
Registered: ‎10-31-2014

AD9154 DAC minimum sample rate, single lane JESD205B question

Hi, Hoping someone can provide some insight into this. I have a customer looking to use the AD9154. http://www.analog.com/en/products/digital-to-analog-converters/high-speed-dac-greaterthan-12msps/ad9... They'd like to run this DAC at 100-200Msps with just one SERDES if possible? It's understood this DAC maybe overkill for the application. However AD9154 could provide a nice upgrade path to high sample rates in future products. Datasheet indicates 300Msps to >2Gsps is DAC update rate with max decimation. I'm also checking with the ADI Eng. Zone. I will update this if/when I get a reply. Thanks, -Spanfan