New Member
Posts: 2
Registered: ‎01-22-2018

Tactrix 2.0 logging analog signal from Zeitronix help


This is my first of many posts.

I got myself a Tactrix 2.0 Cable, and I know the stereo jack input (2.5mm jack) can be hooked up to the serial output from a LC-1/LM-1 and log AFR.

Is there anyway, or does anyone know, if one can use this stereo jack input to log a 0-5V value to the SD card?
I already have a Zeitronix Wideband setup, and it has a 0-5V AFR output (9AFR-20AFR scaled).

Is this at all possible?
Hope someone can point me in the right direction.


I didn't find the right solution from the internet.

Explainer Video Production