Reply
Regular Visitor
Posts: 5
Registered: ‎05-13-2015

AES-XLX-V5LX-EVL110-G

[ Edited ]

Hello

I have a problem with AES-XLX-V5LX-EVL110-G

when I implement of following examples

V5LX Evaluation Boot Loader Example Design
V5LX Evaluation Interrupt Example Design
V5LX Evaluation Xilinx Micro Kernel (XMK) Example Design
V5LX Evaluation lwIP Web Server Example Design
V5LX Evaluation System ACE Module Example Design

in part of programming fpga for Jtag, i have folloguin error:

Creating backup of last automatically saved project to 'C:\Xilinx\14.3\ISE_DS\ISE\auto_project_1.ipf'.
Enumerating cables. Please wait.
Connecting to cable (Usb Port - USB21).
Checking cable driver.
Driver file xusb_emb.sys found.
Driver version: src=1029, dest=1029.
Driver windrvr6.sys version = 10.2.1.0. WinDriver v10.21 Jungo (c) 1997 - 2010 Build Date: Aug 31 2010 x86_64 64bit SYS 14:14:44, version = 1021.
=======================================================
Found cable - > ESN device is not available for this cable.
No ESN.
=======================================================
Connecting to cable (Usb Port - USB22).
Checking cable driver.
Driver file xusb_emb.sys found.
Driver version: src=1029, dest=1029.
Driver windrvr6.sys version = 10.2.1.0. WinDriver v10.21 Jungo (c) 1997 - 2010 Build Date: Aug 31 2010 x86_64 64bit SYS 14:14:44, version = 1021.
ERROR:iMPACT - Cable not found, ESN: 00000000000000
INFO:iMPACT - Failed to open file: -- File ? --, replace with 'bypass'.
INFO:iMPACT:501 - '1': Added Device unknown successfully.
----------------------------------------------------------------------
----------------------------------------------------------------------
INFO:iMPACT - Failed to open file: -- File ? --, replace with 'bypass'.
INFO:iMPACT:501 - '2': Added Device UNKNOWN successfully.
----------------------------------------------------------------------
----------------------------------------------------------------------
INFO:iMPACT - Failed to open file: -- File ? --, replace with 'bypass'.
INFO:iMPACT:501 - '3': Added Device UNKNOWN successfully.
----------------------------------------------------------------------
----------------------------------------------------------------------
Active mode is BS
Loading collection Untitled.
Design rev0 Version 0.
Design rev1 Version 1.
Project: 'C:\Xilinx\14.3\ISE_DS\ISE\auto_project.ipf' loaded.
GUI --- Auto connect to cable...
INFO:iMPACT - Digilent Plugin: Plugin Version: 2.4.3
INFO:iMPACT - Digilent Plugin: no JTAG device was found.
AutoDetecting cable. Please wait.
*** WARNING ***: When port is set to auto detect mode, cable speed is set to default 6 MHz regardless of explicit arguments supplied for setting the baud rates
PROGRESS_START - Starting Operation.
Connecting to cable (Usb Port - USB21).
Checking cable driver.
Driver file xusb_emb.sys found.
Driver version: src=1029, dest=1029.
Driver windrvr6.sys version = 10.2.1.0. WinDriver v10.21 Jungo (c) 1997 - 2010 Build Date: Aug 31 2010 x86_64 64bit SYS 14:14:44, version = 1021.
Cable PID = 0008.
Max current requested during enumeration is 74 mA.
Type = 0x0004.
Cable Type = 3, Revision = 0.
Setting cable speed to 6 MHz.
Cable connection established.
Firmware version = 1303.
File version of C:/Xilinx/14.3/ISE_DS/ISE/data/xusb_xlp.hex = 1303.
Firmware hex file version = 1303.
PLD file version = 0012h.
PLD version = 0012h.
PROGRESS_END - End Operation.
Elapsed time = 1 sec.
Type = 0x0004.
ESN device is not available for this cable.
Attempting to identify devices in the boundary-scan chain configuration...
INFO:iMPACT - Current time: 22/09/2015 10:34:18
PROGRESS_START - Starting Operation.
----------------------------------------------------------------------
----------------------------------------------------------------------
----------------------------------------------------------------------
----------------------------------------------------------------------
Identifying chain contents...INFO:iMPACT:1588 - '0':The part does not appear to be Xilinx Part.
'0': : Manufacturer's ID =Unknown , Version : 10
INFO:iMPACT:501 - '1': Added Device UNKNOWN successfully.
----------------------------------------------------------------------
----------------------------------------------------------------------
'1': : Manufacturer's ID = Unknown
INFO:iMPACT:501 - '1': Added Device UNKNOWN successfully.
----------------------------------------------------------------------
----------------------------------------------------------------------
INFO:iMPACT:1588 - '2':The part does not appear to be Xilinx Part.
'2': : Manufacturer's ID =Unknown , Version : 15
INFO:iMPACT:501 - '1': Added Device UNKNOWN successfully.
----------------------------------------------------------------------
----------------------------------------------------------------------
done.
PROGRESS_END - End Operation.
Elapsed time = 0 sec.

use this programmer https://www.digilentinc.com/Products/Detail.cfm?NavPath=2,395,716&Prod=XUP-USB-JTAG

can you help me? 

thanks

Leo