Reply
Regular Visitor
Posts: 5
Registered: ‎05-13-2015

Impact problem with AES-XLX-V5LX-EVL110-G

[ Edited ]

Hello

I have a problem

 

GUI --- Auto connect to cable...
INFO:iMPACT - Digilent Plugin: Plugin Version: 2.4.3
INFO:iMPACT - Digilent Plugin: no JTAG device was found.
AutoDetecting cable. Please wait.
*** WARNING ***: When port is set to auto detect mode, cable speed is set to default 6 MHz regardless of explicit arguments supplied for setting the baud rates
PROGRESS_START - Starting Operation.
Connecting to cable (Usb Port - USB21).
Checking cable driver.
Driver file xusb_emb.sys found.
Driver version: src=1029, dest=1029.
Driver windrvr6.sys version = 10.2.1.0. WinDriver v10.21 Jungo (c) 1997 - 2010 Build Date: Aug 31 2010 x86_64 64bit SYS 14:14:44, version = 1021.
Cable PID = 0008.
Max current requested during enumeration is 74 mA.
Type = 0x0004.
Cable Type = 3, Revision = 0.
Setting cable speed to 6 MHz.
Cable connection established.
Firmware version = 1303.
File version of C:/Xilinx/14.3/ISE_DS/ISE/data/xusb_xlp.hex = 1303.
Firmware hex file version = 1303.
PLD file version = 0012h.
PLD version = 0012h.
PROGRESS_END - End Operation.
Elapsed time = 0 sec.
Type = 0x0004.
ESN device is not available for this cable.
Attempting to identify devices in the boundary-scan chain configuration...
INFO:iMPACT - Current time: 13/08/2015 15:47:43
PROGRESS_START - Starting Operation.
Identifying chain contents...'0': : Manufacturer's ID = Unknown
INFO:iMPACT:501 - '1': Added Device UNKNOWN successfully.
----------------------------------------------------------------------
----------------------------------------------------------------------
INFO:iMPACT:1588 - '1':The part does not appear to be Xilinx Part.
'1': : Manufacturer's ID =Unknown , Version : 5
INFO:iMPACT:501 - '1': Added Device UNKNOWN successfully.
----------------------------------------------------------------------
----------------------------------------------------------------------
INFO:iMPACT:1588 - '2':The part does not appear to be Xilinx Part.
'2': : Manufacturer's ID =Unknown , Version : 15
INFO:iMPACT:501 - '1': Added Device UNKNOWN successfully.
----------------------------------------------------------------------
----------------------------------------------------------------------
done.
PROGRESS_END - End Operation.
Elapsed time = 1 sec.

 

Can you help me? 

Regular Visitor
Posts: 5
Registered: ‎05-13-2015

Re: Impact problem with AES-XLX-V5LX-EVL110-G

hi, I have same problem and use this programmer https://www.digilentinc.com/Products/Detail.cfm?NavPath=2,395,716&Prod=XUP-USB-JTAG thanks