Reply
Newbie
Posts: 1
Registered: ‎10-11-2013

7" Zed Touch Display Kit - Linux framebuffer use, without X11

Where would I find info on how to get this display working under Linux (xilinx-v14.6.02) with a framebuffer (no X11). 

 

We've got our PL updated with the AXI VDMA device, and the stand-alone/baremetal Controller/Console apps work fine, but our system is Linux-based, running Qt.

 

Where I'm at now, the following info is in the bootup messages:

 

...

xilinx-vdma 43000000.axivdma: Probing xilinx axi vdma engine
xilinx-vdma 43000000.axivdma: unable to request IRQ

....

 

Once it boots, there's no /dev/fb0.

 

Trying to learn where to go from there.

Thanks

Avnet Employee (Star Contributor)
Posts: 114
Registered: ‎06-09-2009

Re: 7" Zed Touch Display Kit - Linux framebuffer use, without X11

Hi kstone,

 

Have you taken a look at "Display Panel Ubuntu Tutorial for ZedBoard" on the Reference Designs/Tutorials page for the Zed Display Kit?

 

http://www.zedboard.org/design/1668/13

 

This tutorial covers adding support for the display to a 3.6 Linux kernel using a patch.

 

Regards,

 

-Kevin