Reply
Regular Contributor
Posts: 34
Registered: ‎03-22-2012

FMC modules for AXI bus

Has Avnet ported the FMC IP to use the AXI bus instead of the older PLB interface that is in all the example apps? Presumably these cores and software libraries only work with the PLB interface given that PLB is in the core names (e.g., SG_I2C_CONTROLLER_PLBW).

 

I want to use the microblaze core with the FMC_IMAGEOV board and OV9715 camera on a Spartan-6 LX150T development board. Once the zedBoards ship to customers, I plan to transition much of this AXI-based IP using the same FMC_IMAGEOV and OV9715 hardware.

 

Bryn Wolfe