Reply
Highlighted
Visitor
Posts: 1
Registered: ‎03-03-2017

FMC-HDMI-CAM-G

Hello - I'm trying to use the FMC-HDMI-CAM-G module to handle HDMI input/output for a project using a Zedboard Zynq-7000 board. I have two questions if anyone can help it would be greatly appreciated:

1. Will any tutorial written for the old FMC IMAGEON work for the FMC-HDMI-CAM-G? I understand the FMC IMAGEON is now obsolete and the FMC-HDMI-CAM-G is the successor module. 

2. It seems that any tutorial that uses tcl scripts for, say vivado 2015.x, will only work if you're using that specific version of Vivado. Is this correct? So if I'm using Vivado 2016.2 then I need to install the specific Vivado version referenced in the tutorial?

Thank you