Reply
New Member
Posts: 2
Registered: ‎02-27-2017

FMC-HDMI-CAM tutorial - tcl script would not finish running

Hi,

I am following the tutorial below but the make tcl script would not finish running. I have Vivado2015.4 and I can see that the licenses are valid at the beginning when the tcl script started. The only file that was created was the .xpr file (out of the three expected files). Then the script would keep running without the other two files created.

ZedBoard + FMC-HDMI-CAM + PYTHON-1300-C Vivado HLS Reference Design, Vivado 2015.4

http://zedboard.org/sites/default/files/design/FMCHC_PYTHON1300C_HLS_2015_4_02_zedboard.zip

Note that the PYTHON-1300-C camera module is optional, and not mandatory.

 

Any pointers on what have gone wrong?

Thanks!

Avnet Employee (Star Contributor)
Posts: 471
Registered: ‎04-16-2009

Re: FMC-HDMI-CAM tutorial - tcl script would not finish running

Can you share the output of your TCL console ?

   Vivado% source ./scripts/create_project.tcl
  
...

Did you try to open the GUI with the following command ?

   Vivado% start_gui

 

Regards,

Mario.