Reply
Regular Visitor
Posts: 1
Registered: ‎12-03-2015

FMC-HMDI Passtrough FMC-IN -> zc702-HDMI-OUT

[ Edited ]

Hello, Im realy new to Zynq design.

I have to implement an video processing design wiht an Xilinx Zynq zc702. But i dont own an FMC-Imageon card. Instead im using a Digilent FMC-HDMI card with only one HDMI-Input.

My question is: Can i use the Passthrough Tutorial to do this? Im changed the constrains to match the pins for Digilent FMC-Card and im getting the information of my source (PC: 1920x1080). But the output monitor stays off and is black. I also change the constrains for the ADV7511 on the zc702 to match the pin mapping in the User Guide (UG850 (v1.5)).

Do i have to change something in my HW-Design?

I attached my TeraTerm output.

Thank you very much!!!

 

 

EDIT: PLEASE CAN ANYONE HELP ME??

 

a.PNG
Visitor
Posts: 1
Registered: ‎06-22-2016

Re: FMC-HMDI Passtrough FMC-IN -> zc702-HDMI-OUT

Hello.

I have the same problem. I have not FMC. 

I use zc702 only and i want to display HD test on the HDMI monitor.

Do you have any success ?

 

 

Highlighted
Newbie
Posts: 1
Registered: ‎11-28-2017

Re: FMC-HMDI Passtrough FMC-IN -> zc702-HDMI-OUT

Hi, I will like to do the same but I don't have any idea how to... Did you finish you Passthrough project?  Any help with the Digilent FMC-HDMI?

Thanks in advance...