Reply
Visitor
Posts: 2
Registered: ‎01-14-2017

FMC-IMAGEON – HDMI Pass-Through Tutorial

Hello all,

I'm a beginner and I'm trying the HDMI pass-through example (2013) on vivado 2016.2, 
when typing the TCL line "source C:/FMC_IMAGEON/2013_3/scripts/fmc_imageon_hdmii_yuv422.tcl"  the IP is generated in the block design but I have an error in the console: 

ERROR: [BD 5-216] VLNV <xilinx.com:ip:xlconstant:1.0> is not supported for the current part. The latest supported version for this part is:1.1
ERROR: [Common 17-39] 'create_bd_cell' failed due to earlier errors.

also, for the VTC-control, I have the following message: no matching connections found for 'vtc-control' interface

please can you explain for me the origin of these errors.

thank you all

Highlighted
Avnet Employee (Star Contributor)
Posts: 471
Registered: ‎04-16-2009

Re: FMC-IMAGEON – HDMI Pass-Through Tutorial

The TCL scripts are not portable from one tool version to another.

The best way to handle this, is to run the tutorial with the appropriate tool version (2013.x), then open the resulting project with the new tool version (2016.x).

Regards,

Mario.