Reply
Avnet Employee (Star Contributor)
Posts: 471
Registered: ‎04-16-2009

FMC-IMAGEON IP Cores and Tutorials for Vivado 2015.4

Hello all,

I have posted a new set of FMC-IMAGEON IP Cores and Tutorials for Vivado 2015.4, which can be accessed on the zedboard.org community website:

   http://microzed.org/sites/default/files/design/FMC_IMAGEON_GettingStarted_2015_4_01.zip

There are also versions for previous versions of the Xilinx tools:

   http://microzed.org/sites/default/files/design/FMC_IMAGEON_GettingStarted_2015_2_01.zip

   http://microzed.org/sites/default/files/design/FMC_IMAGEON_GettingStarted_2014_4_01.zip

   http://microzed.org/sites/default/files/design/FMC_IMAGEON_2013_3_IP_Tutorials_20140320%281%29.zip

Regards,

Mario.

Visitor
Posts: 4
Registered: ‎04-26-2016

Re: FMC-IMAGEON IP Cores and Tutorials for Vivado 2015.4

[ Edited ]

Hi,

I followed the Getting Started guide for 2015.2, I'm getting the following error: "VITA sensor failed to initialize".

This is my setup: a MicroZed board with the Embedded Vision Card and the Avnet Python camera module. In the TCL script, I commented out everything except the last 3 lines (to compile for the Microzed-7020 + FMC Carrier Card).

Any idea of what could be the problem?

Avnet Employee (Star Contributor)
Posts: 471
Registered: ‎04-16-2009

Re: FMC-IMAGEON IP Cores and Tutorials for Vivado 2015.4

Esaias,

The following are different hardware platforms :

- MicroZed Embedded Vision Kit => supports the PYTHON-1300-C camera module

- FMC-IMAGEON => FMC module supporting the VITA-2000-C camera module

You cannot mix and match the ref designs for different hardware ...

If you have a MicroZed Embedded Vision Kit, then you need to use ref designs for this kit. 

In your case, you should be using the following:

http://microzed.org/sites/default/files/design/EMBV_PYTHON1300C_Frame_Buffer_Tutorial_2015_4_01.zip

http://microzed.org/sites/default/files/design/EMBV_PYTHON1300C_Frame_Buffer_Tutorial_2015_2_01.zip

Regards,

Mario.

Visitor
Posts: 4
Registered: ‎04-26-2016

Re: FMC-IMAGEON IP Cores and Tutorials for Vivado 2015.4

No wonder it doesn't work! Thank you, I'll give it a try.

Regular Visitor
Posts: 3
Registered: ‎09-19-2012

Re: FMC-IMAGEON IP Cores and Tutorials for Vivado 2015.4

Hi!

New 2015.4 version for FMC-HDMI-CAM was uploaded too.

http://picozed.org/sites/default/files/design/FMCHC_PYTHON1300C_Tutorial_2015_4_01.zip
http://picozed.org/sites/default/files/design/FMCHC_PYTHON1300C_HLS_2015_4_01.zip

It seems that second one (with HLS) is broken.

Could you check it ?

Thanks a lot!
Highlighted
Regular Visitor
Posts: 5
Registered: ‎12-06-2014

Re: FMC-IMAGEON IP Cores and Tutorials for Vivado 2015.4

Sorry for bothering but I can not download these zip files. I registered my account on ZEDBOARD.ORG yesterday. When I click on the 'Download' button a redirect link appears (http://zedboard.org/restrict/download/redirect?redirect=/sites/default/files/design/FMC_IMAGEON_Gett...). So, could you send these zip files to my email ? It's nolaziness@zju.edu.cn . Thanks.
Newbie
Posts: 1
Registered: ‎03-16-2018

Re: FMC-IMAGEON IP Cores and Tutorials for Vivado 2015.4

Hello,

I'm trying to follow these tutorial for a college project, but I can only find 2013.3 IP Tutorials files. Not just the getting started files.

The computers have Vivado 2014.4 installed. Where can I get the IP tutorials files for that version?

 

regards,

 

Alex.