Reply
Newbie
Posts: 1
Registered: ‎02-11-2016

mistake with fifo_generator_v12_0

Hi,

I work on the getting started design tutorial (FMC-IMAGEON + VITA-2000-C). This tutorial is for the vivado's version 2014.4, but I use vivado 2015.4.

I passed to create the fmc_imageon_gs design, the synthesis was complete, but the implementation failed and write the folowing error :

  • [DRC 23-20] Rule violation (INBB-3) Black Box Instances - Cell 'fmc_imageon_gs_i/onsemi_vita_cam_0/U0/onsemi_vita_cam_v3_1_S00_AXI_inst/onsemi_vita_cam_core_inst/framestart2_regen_l/pulse_regen_l' of type 'fmc_imageon_gs_i/onsemi_vita_spi_0/U0/onsemi_vita_spi_v3_1_S00_AXI_inst/onsemi_vita_spicore_inst/vita_spi_txfifo_l/afifo_32_l/fifo_generator_v12_0' has undefined contents and is considered a black box. The contents of this cell must be defined for opt_design to complete successfully.

How can I resolve my project?

Thanks

Bye! 

New Member
Posts: 2
Registered: ‎03-04-2016

Re: mistake with fifo_generator_v12_0

In 2015.4, fifo generator v13 is used. You have to updated IP accordingly.
Avnet Employee (Star Contributor)
Posts: 471
Registered: ‎04-16-2009

Re: mistake with fifo_generator_v12_0

Christophe,

I have posted a new version of the design for Vivado 2015.4.

https://www.em.avnet.com/Support%20And%20Downloads/FMC_IMAGEON_GettingStarted_2015_4_01.zip 

Regards,

Mario.

Newbie
Posts: 1
Registered: ‎05-21-2017

Re: mistake with fifo_generator_v12_0

Hi,

   How about the 2016.4 because I have the same problem on Vivado 2016.4.

thanks.