Reply
Visitor
Posts: 2
Registered: ‎06-18-2013

Ethernet MAC not working in PL side for Zed Board!

Hi,

I am trying to implement a soft EMAC (100Mbps) and using FMC -ISMNET card . I have done the connections for TX and RX side including reset, powerdown etc. as per the documentation.

I am running loopback test using the peripheral test application generated in SDK. The application hangs on loopback test.

Anyone having suggestion on this....

 

Thanks,
Ved

Visitor
Posts: 2
Registered: ‎06-18-2013

Re: Ethernet MAC not working in PL side for Zed Board!

Hi,

 

Just want to update that  Tx side i can see data packets being sent but on Recieve side ,no response is there in the loopback test.

 

Thanks,

Ved

Highlighted
Visitor
Posts: 2
Registered: ‎09-05-2013

Re: Ethernet MAC not working in PL side for Zed Board!

Hi,

did you solved your issue about the using the ISM networking ethernet connector with the axi_ethernet IP?

I am currently facing the same issue with ISM networking card  plugged onto a KC705 board. I am setting the axi_ethernet IP in MII mode, and I have connected a GPIO to set the powerdown pin to 1 in the way to have the transceivers power on. and no LED is on and then the self test in DMA mode doesn't work...

Any help is welcomed.

Is there an basic example available for the ISM module using the axi_ethernet Ip form XILINX?

Regards,

Julien