Reply
Highlighted
Newbie
Posts: 1
Registered: ‎11-19-2018

Epson Printer Offline Windows 10

How to Fix Epson Printer Offline Windows 10 Simple Steps

Troubleshoot Epson printer offline error
There seems to be a recurring issue with users of Windows 10 showing Epson printer Offline even after they install all required drivers for their Epson printer Offline Support. If you are one of those experiencing this problem, then you can start troubleshooting this error by first checking the hardware device.

Fix Printer Offline Issues Toll Free Call US- +1-844-669-3399

 

Checking your Epson Printer hardware

  1. Obvious as it may seem, first you need to ensure that the printer is on, most models will have some sort of light to notify you of this
  2. If you are using a wired printer, ensure the printer cable is properly connected to the computer. You should check the connections at both ends to ensure they are firmly seated and check the cable itself for any obvious damage
  3. If you are using a wireless printer, ensure it is connected to the network. You can check the wireless connection of your Epson printer by running the printer’s wireless connectivity test. Follow the steps below to get the printer status/connection report
  4. Enter Setup Mode
  5. Select Network Settings
  6. Select Confirm Network Settings
  7. Confirm the connection status
  8. Take a note of the IP address of the printer (which means it is connected)
  9. If you want to print the status report, press Start. Your Epson printer will now print the Printer status page

Need Help Call US- +1-844-669-3399