Reply
Highlighted
New Member
Posts: 3
Registered: ‎09-25-2018

QuickBooks Error Code 6129, 0 – A Complete Solution Procedure

A common QuickBooks error code usually appear in front of the QB users that is – QuickBooks Error Code 6129, 0. This error code could possible appear when the database connection verification fails or while accessing the QB company files. In this post, we are going to discuss about the QuickBooks Error 6129, 0 along with its solution. In case, you need help of the expert – we suggest you to take support from the QuickBooks Help Services.

 

Causes of QuickBooks Error 6129, 0

Check out the possible reasons due to which the QuickBooks Error 6129, 0 occurs:-

  • When the entire machines are using the multi-user aptitude & the latest QB update is absent.
  • When the data files are present on the corrupt network.
  • Due to mismatch between the client & server domain.
  • Missing, damaged, or co0rrupt QB files or QuickBooks Installation.

 

Solution Steps for QB Error Code 6129, 0

  • Updating the company file
  • Conduct easy exit from QuickBooks
  • Disable the anti-virus program
  • Rename the QuickBooks Network Descriptor Files
  • Navigate the QuickBooks Company File
  • Activate one domain

 

If you seek assistance of the QuickBooks professional to deal with this problem..!! You can contact us at our QuickBooks Toll free Helpline Number .i.e. +1-800-880-6389. We remain active 24/7 to provide you a world class services.