Reply
Avnet Employee
Posts: 4
Registered: ‎12-12-2014

RF GAN Power Amplifier >50W

What suppliers do we have on our linecard for RF GaN Power Amplifier, wideband (ideally 500MHz - 6GHz) and anywhere from P1db= 50W to 300W?

NXP has a very limited offering. Any others?

 

Regards,

Flavio

Highlighted
Avnet Employee (Regular Contributor)
Posts: 35
Registered: ‎12-01-2014

Re: RF GAN Power Amplifier >50W

Hello Flavio:

Not knowing your specific application or customer type, you may want to consider speaking with our Supplier E2V.  E2V has partnered with GaN Systems to provided Hi Reliabiity and Space grade GaN MOSFETs.  I've attached a brief presentation for this.  Note that these won't compete on PRICE with commercial GaN from EPC, or even GaN Systems but it is a solution that we can offer if the customer needs this value. 

See Attached!

Hope this Can Help You!

DeWayne Gibson