Reply
New Member
Posts: 2
Registered: ‎11-21-2018

Sbcglobal Email not Working Problem

Main Reasons for SBCGlobal Email Problems

There are plenty of causes which are responsible for the arrival of this email services such as

  • When the internet is not connected to your system in a straightforward way, then you cannot access SBC Global email services.
  • If you are sending the emails to wrong email recipients.
  • You are trying to send the emails to the blocked email address.
  • Firewall and Antivirus software settings prevent the users to send and receive the emails.
  • When there is a problem in the servers, then this can create this technical issue.
  • This problem can also appear due to problems in the settings of an email account.
  • When the browser is not supportive and becomes outdated, then it can also create this error.

Symptoms:

  • Slow loading of the emails
  • Frequent pop-up of an email error message on the Windows screen
  • Cannot send and receive the emails
  • Unable to access SBCGlobal e-mail
  • Spamming of the messages

Steps to Fix 5 Most Common SBCGlobal Email Problems

  • Resolve Sending and Receiving the Emails: You can troubleshoot this technical issue by checking the folders of outbox and sent file of the email. Besides, it is advisable to check the settings of your email account.
  • Missing of any Mails and Slow Loading of the Emails: This happens can also appear due to an outdated or obsolete version of SBCGlobal email. It is essential to update the current browser, which will help you in resolving this problem.
  • Missing Contacts and Mails: Submit the request of the server to recover the lost contacts and restore the email accounts.
  • Spamming of Emails: In order to avoid the unwanted emails, then you should block such email addresses.
  • Fix Sign in Problems: Entering the wrong email password is one of the foremost reasons for the arrival of this problem. In order to fix this issue, you should enter the correct email password.

Source : Sbcglobal Email Not working