Reply
Highlighted
Newbie
Posts: 1
Registered: ‎04-15-2013

how to run a DMA(OCM2PL.c) on linux environment as s/w using zed board

I followed same procedure as like as simple Hello_world mention in zedboard and chosen "OS Platform as Linux".check out this link i followed the procedure as
http://zedboard.org/content/zedboard-create-planahead-project-embedded-p....
Then replaced that Hello_world code by My program(DMA).I attached the DMA program.please refer this one.while compling I faced error and post in the zedboard->support->s/w development application and then as u said i added header files in the project explorer window in SDK to the include folder as a path.pls check out link below for header file inclusion as http://s1322.photobucket.com/user/Arunvision/media/sdk_bsp_zps99084a46.j...

 

we got the error like as

 

 

**** Build of configuration Debug for project Dma ****

make all
Building file: ../src/OCM2PL.c
Invoking: ARM Linux gcc compiler
arm-xilinx-linux-gnueabi-gcc -Wall -O0 -g3 -I"C:\Xilinx\14.4\ISE_DS\EDK\sw\XilinxProcessorIPLib\drivers\scutimer_v1_00_a\src\" -I"C:\Xilinx\14.4\ISE_DS\EDK\sw\XilinxProcessorIPLib\drivers\dmaps_v1_00_a\src" -I"C:\Xilinx\14.4\ISE_DS\EDK\sw\XilinxProcessorIPLib\drivers\scugic_v1_00_a\src" -I"C:\Xilinx\14.4\ISE_DS\EDK\sw\XilinxProcessorIPLib\drivers\common_v1_00_a\src" -I"C:\Xilinx\14.4\ISE_DS\EDK\sw\lib\bsp\standalone_v3_07_a\src\cortexa9" -c -fmessage-length=0 -MMD -MP -MF"src/OCM2PL.d" -MT"src/OCM2PL.d" -o"src/OCM2PL.o" "../src/OCM2PL.c"
arm-xilinx-linux-gnueabi-gcc: fatal error: no input files
compilation terminated.
make: *** [src/OCM2PL.o] Error 1

 

 

Pls provide solution as soon as possible.

Avnet Employee (Star Contributor)
Posts: 114
Registered: ‎06-09-2009

Re: how to run a DMA(OCM2PL.c) on linux environment as s/w using zed board

Hi swapna,

 

These forums here are for Avnet branded boards only.  Although ZedBoard is technically an Avnet board, it is a community board and so we ask that you post questions to the ZedBoard.org site for the benefit of the rest of the ZedBoard.org community.

 

Is this your ZedBoard.org forum post?

 

http://www.zedboard.org/content/how-run-dma-program-linux-environment-using-zed-board

 

If you are not satisfied with the response on the ZedBoard.org forums, please respond back to your original post on the ZedBoard.org forums and clarify your problem further by asking for assistance on specific topics.  Duplicating forum posts in multiple locations while attempting to solicit feedback from multple sources circumvents the spirit of the community we are trying to foster on the ZedBoard.org website.  

 

Thank you for your patience and understanding.

 

Regards,

 

-Kevin