Reply
Highlighted
Regular Contributor
Posts: 33
Registered: ‎04-14-2009

PSOC

What is a Cypress PSOC
Administrator
Posts: 43
Registered: ‎04-13-2009

Re: PSOC

The Cypress PSOC stands for Programmable System On a Chip. However, it's much more. It's one of the only programmable mixed signal devices. Not only does it have an internal microcontroller, but it has extensive programmable analog elements.
Newbie
Posts: 1
Registered: ‎05-15-2009

Re: PSOC - where's the example?

Junegirl,

 

I followed the instructions that came with the Spartan 3A kit, stating to download PSoC 5.0 from the Cypress website, and then open PSoC and the example. Could you please tell me where to find the example?

 

 

Greg Taylor, P.E.

Avnet Employee (Star Contributor)
Posts: 128
Registered: ‎04-20-2009

Re: PSOC - where's the example?

Hi Greg,

 

Here is where you can download it:

 

http://www.cypress.com/?rID=34517

 

John

Visitor
Posts: 6
Registered: ‎06-27-2012

Re: PSOC - where's the example?

The Cypress PSoC 1 (Programmable System-on-Chip) integrates a microcontroller with programmable analog and digital peripherals. Use the AN75320 application note to get started on the capabilities of PSoC 1 devices and the PSoC Designer development environment used to configure and program those devices.

[http://www.cypress.com/?rID=58639]

Visitor
Posts: 4
Registered: ‎10-14-2018

Re: PSOC - where's the example?

[ Edited ]

@Anshul wrote:

The Cypress PSoC 1 (Programmable System-on-Chip) integrates a microcontroller with programmable analog and digital peripherals. ShowBox Mobdro TutuApp Use the AN75320 application note to get started on the capabilities of PSoC 1 devices and the PSoC Designer development environment used to configure and program those devices.

[http://www.cypress.com/?rID=58639]


It's one of the main programmable blended flag gadgets. In addition to the fact that it has an inside microcontroller, it has broad programmable simple components.