06-08-2016 12:05 PM
I am trying to follow the quickstart guide for the 7A50T board. I installed the UART driver from the link on the quickstart guide. It says it was sucessful and shows up under device manager. When I configure realterm to use this port with the 115200 8 bits 1 stop bit no parity settings mentioned in the quickstart guide I am unable to see any sucessful transmission when pushing switch 8. Also realterm is indicating that there is a "break" condition.
Any suggestions on how to get the UART to USB working for the demo on 7A50T eval board would be much appreicated
07-13-2016 09:08 AM
Simple question but perhaps very inportant. What bit file is loaded into the FPGA? You need to insure that you have a design loaded that has a UART in it.
Nick