Reply
Visitor
Posts: 3
Registered: ‎05-11-2016

AES-A7EV-7A50T: 7A50T OOB Design Problem

Hello,

 

when importing the OOB Design in Vivado 2015.4 or 2016.1 i receive the error that the files mig_a.prj and mig_b.prj are missing:

[Project 1-311] Could not find the file 'C:/Users/Pongratz/Documents/Xilinx_Vivado/7A50T_OOB_Design_VIV2014_1_orig/IPI/7A50T_OOB_Design.srcs/sources_1/bd/MB_System/ip/MB_System_mig_7series_0_1/mig_a.prj', nor could it be found using path 'C:/Projects/DRC_Dev/7A50T_OOB_Design_VIV2014_1/IPI/7A50T_OOB_Design.srcs/sources_1/bd/MB_System/ip/MB_System_mig_7series_0_1/mig_a.prj'.

[Project 1-311] Could not find the file 'C:/Users/Pongratz/Documents/Xilinx_Vivado/7A50T_OOB_Design_VIV2014_1_orig/IPI/7A50T_OOB_Design.srcs/sources_1/bd/MB_System/ip/MB_System_mig_7series_0_1/mig_b.prj', nor could it be found using path 'C:/Projects/DRC_Dev/7A50T_OOB_Design_VIV2014_1/IPI/7A50T_OOB_Design.srcs/sources_1/bd/MB_System/ip/MB_System_mig_7series_0_1/mig_b.prj'.

 

The file mig_a.prj is available in another version of the IP (MB_System_mig_7series_0_0) but the mig_b.prj file is nowhere in the folders of the project. Are these files curcial for the demo design?

 

Thanks & BR

Martin

Avnet Employee (Super Contributor)
Posts: 79
Registered: ‎04-17-2009

Re: AES-A7EV-7A50T: 7A50T OOB Design Problem

Hi Martin,

I will look into these error messages and get back to you.  I may need to recreate the OOB design for Vivado 2015.4.  Stay tuned.

 

Regards,

Tom

--
Tom Curran
Newbie
Posts: 1
Registered: ‎07-24-2018

Re: AES-A7EV-7A50T: 7A50T OOB Design Problem

This kind of error is something new too me, did you get a solution and also a reason why this happened? If yes do let me know too so I can be prepared in case of any such bugs/errors.

With Regards,
Zagakuf Sen

Plex Tutuapp Vidmate