Reply
cas
Visitor
Posts: 1
Registered: ‎09-21-2015

Artix 7A50T Demo Programming Problems

Please can somebody tell me Vivado 2015.1 will support this demo card?

When i try to use the Vivado Hardware Manager to connect to the target it acts as if there is no target available.

The USB to UART driver is loaded. Any clues what i need to do?

 

Avnet Employee
Posts: 2
Registered: ‎10-18-2010

Re: Artix 7A50T Demo Programming Problems

The Arty board is supported in Vivado 2015.1. I just tried it. Are you able to programm the FPGA using the hardware manager? Did you try reinstalling the driver?

 

-Dieter