Reply
Visitor
Posts: 3
Registered: ‎04-27-2016
Accepted Solution

BPI bootloader example for Kintex-7 MMP

Hello,

We have a Kintex-7 MMP kit (AES-MMP-7K325T).  We have finished a hardware design which includes a MicroBlaze and a software application for this design, now we want to program the bitstream and elf file to the MMP flash.   The user guide of Kintex-7 MMP (5331-UG-AES-XK7MMP-G-V1_3) only provides how to do it by using ISE iMPACT, but we want to know how to do it by using VIVAD/SDK.  We alos fond a document "5185-7A35T-Arty-SREC-Bootloader-VIV2015-2-V1" which described how to create a bootloader for Arty board, but it is for a QSPI flash. 

Is there any tutorial for programming flash on Kintex-7 MMP by using VIVADO/SDK?  or any document like "5185-7A35T-Arty-SREC-Bootloader-VIV2015-2-V1" but for programming on a BPI flash?

 

Best,

bj

Highlighted
Avnet Employee (Star Contributor)
Posts: 511
Registered: ‎05-05-2009

Re: BPI bootloader example for Kintex-7 MMP

Here is a Vivado/SDK Bootloader example design https://avnet.egnyte.com/dl/0yF4i4gOes.

 

Visitor
Posts: 3
Registered: ‎04-27-2016

Re: BPI bootloader example for Kintex-7 MMP

Thank npoureh for the information.  I've done the bootloader example.  But in that example, it only shows how to generate a bootloader application and run it as launched on hardware.  It lacks futher instructions about how to integrate the bootloader elf with FPGA bitstream and to download the integrated bitstream to the board.  Alos it lacks how to setup constraints properly for BPI configuration to generate the bitstream for the Kintex-7 MMP.   So this example design does not solve our problem.

I consulted the following reference:

  • XAPP1220,
  • Avnet Kintex-7 MMP Embedded Design,
  • SPI SREC Bootloader Example Design for the Arty Evaluation Board,

and made some progress.  At Vivado side, I used following constraints for BPI configuration to create the bitstream for Kintex-7 MMP:

        set_property CONFIG_VOLTAGE 2.5 [current_design]

        set_property CFGBVS VCCO [current_design]

        set_property BITSTREAM.GENERAL.COMPRESS TRUE [current_design]

        set_property BITSTREAM.CONFIG.EXTMASTERCCLK_EN DIV-1 [current_design]

        set_property BITSTREAM.CONFIG.BPI_SYNC_MODE TYPE2 [current_design]

        set_property CONFIG_MODE BPI16 [current_design]

At SDK side, I did following steps:

  1. run "Program Flash" to write my application into flash memory.  The offset was set as 0x00600000; flash type was set "28f512p30t-bpi-x16"; the "Convert ELF to SREC" option was ticked.
  2. A bootloader application was made based on SREC Bootloader templates, and set the FLASH_IMAGE_BASEADDR as 0x60600000.  
  3. Run the "Program FPGA" including the bootloader elf to generate the downlad.bit.

So far, the MMP worked fine.  I saw the bootloader was working after FPGA being programmed, and my application being loaded successfully by bootloader.  Following message showed at terminal.

        SREC Bootloader

        Loading SREC image from flash @ address: 60600000

        ...

        Executing program starting at address: 00000000

Next, I run "Program Flash" again to write the download.bit into flash (the offset was set as 0x00000000), then turned off and turned on the MMP power.  The bootloader looked work after MMP power on, but I got an error message:

        SREC Bootloader

        Loading SREC image from flash @ address: 60600000

        ERROR: Error while reading an SREC line from flash

If I re-run "Program FPGA" to write FPGA bitstream with bootloader elf as the step 3 shown above,  the design was work fine again.

Can anyone helps on this "Error while reading an SREC line from flash" problem?

 

best,

bj

Visitor
Posts: 3
Registered: ‎04-27-2016

Re: BPI bootloader example for Kintex-7 MMP

Hi,

I find a solution to solve "Error while reading an SREC line from flash" problem.  It is due to the failure of bitstream booting in synchronous mode.  The details can be found in the "VC709 BPI unreadable after boot" topic in Xilinx community forms (https://forums.xilinx.com/t5/Xilinx-Boards-and-Kits/VC709-BPI-unreadable-after-boot/td-p/566033).

 

In my case, I modifed the BPI configuration constraints as follows

       set_property CONFIG_VOLTAGE 2.5 [current_design]

        set_property CFGBVS VCCO [current_design]

        set_property BITSTREAM.GENERAL.COMPRESS TRUE [current_design]

        set_property BITSTREAM.CONFIG.EXTMASTERCCLK_EN DISABLE [current_design]

        set_property BITSTREAM.CONFIG.BPI_SYNC_MODE DISABLE [current_design]

        set_property CONFIG_MODE BPI16 [current_design]

The modifications are labeled by bold font.  Then we re-generate the bitstream file by using these constriants on Vivado.  The download.bit file integrated by this new bitstream and bootloader elf is work fine after it being programmed into the MMP flash.

best,

bj