Posts: 1
Registered: ‎01-04-2017

MMP - MAC Address programmed in PHY


Can anyone provide details about whether or not the phy that comes with the MMP is pre-configured with a unique MAC or this needs to be provided by us.

The reported MAC, by default, has a Xilinx vendor ID (00:0A:35) however I did not see any information in the documentation suggesting if this is fully unique or we need to program ourselves.



Avnet Employee (Star Contributor)
Posts: 511
Registered: ‎05-05-2009

Re: MMP - MAC Address programmed in PHY

MMP is not shipped with a unique MAC Address, user needs to provide it.