Reply
Newbie
Posts: 1
Registered: ‎03-08-2016

PicoZed questions

We plan on using the PicoZed kit:

http://www.xilinx.com/products/boards-and-kits/1-askjht.html

 

1) It shows that the band is 70MHz to 6GHz.  We were wondering if the kit is ever run up to 6GHz or rather, is it practical.  What's the typical operating range?   

 

2) I got the user's manual 1.2 and near the end it states that the datasheet uses narrowband baluns while the test uses wideband baluns for the PicoZed SDR Z7035/AD9361.  Is it confirmed that this model uses wideband baluns (or both)? 

 

3) Where can we find a footprint of the chip?  I don't think the manual has a clear one. 

 

Thanks!

 

Highlighted
Avnet Employee (Star Contributor)
Posts: 106
Registered: ‎07-07-2009

Re: PicoZed questions

This conversation has been moved here -- http://picozed.org/content/picozed-questions

 

/Matt