Reply
Highlighted
Visitor
Posts: 3
Registered: ‎11-05-2018

Regarding ISM Networking Module II

Can the - ISM Networking Module II be used for Ethernet applications, not industrial ethernet. Also, are there other boards available that can be used for the purpose of ethernet

Thanks

Avnet Employee (Star Contributor)
Posts: 111
Registered: ‎07-07-2009

Re: Regarding ISM Networking Module II

The ISM Networking Module II is not limited in any way to Industrial applications.

You might also want to consider our recently announced Network FMC card.

See below for a summary of features for both cards.

Network FMC

  • Dual 10/100/1000 Mbps (RGMII) Ethernet interfaces
  • Microchip KSZ9031RNX PHY
  • No backward compatibility with Avnet’s FMC-ISMNET2 module
  • I/O voltages of 1.8V, 2.5V and 3.3V supported
  • Product page
  • Avnet Reference Designs:
    • UltraZed-EG PCIe Carrier Card

 

ISM Networking Module II

  • Dual IEEE 1588 10/100 Mbps (MII/RMII) Ethernet interfaces
  • Texas Instruments DP83640TVV PHY
  • Dual CAN, plus single RS-232 and RS-485 interfaces
  • Pin compatible with previous version (AES-FMC-ISMNET-G)
  • I/O voltage limited to 2.5V and 3.3V; 1.8V is not supported
  • Avnet Reference Designs: n/a
  • Product Page
  • 3rd Party Reference Designs:
    • Industrial Ethernet on MicroZed Industry 4.0 Ethernet Kit
    • HSR/PRP on MicroZed Industry 4.0 Ethernet Kit
Newbie
Posts: 1
Registered: ‎12-18-2018

Re: Regarding ISM Networking Module II

Get ready for the new Publix Weekly Ad! The Publix weekly ad circular and next week’s Publix ad are posted here! Don’t miss out on any new Publix weekly specials which often includes Publix weekly ad bogo sales! bi-lo weekly specials

Newbie
Posts: 1
Registered: ‎01-04-2019

Re: Regarding ISM Networking Module II

The Blue Tigers have participated in Asia's top football competition thrice before, with their best performance coming way back in 1964, during the Golden Era of Indian football, when the team finished as AFC Asian Cup 2019 Live Online

Though the Stephen Constantine-coached side failed to qualify for the World Cup, they managed to reach the third round of the 2019 AFC Asian Cup qualifiers thanks to their 7-1 (AGG) drubbing of Laos in Round 1 of the play-off round.