Reply
Newbie
Posts: 1
Registered: ‎09-12-2011

Parallel Cable III Part No. HW-JTAG-PC Software

I have a legacy Parallel Cable III Part No. HW-JTAG-PC The cable is also used to program FPGA's.

I'm currently looking for the software. Does anyone know where I can download the software.

Highlighted
Avnet Employee (Star Contributor)
Posts: 614
Registered: ‎04-20-2009

Re: Parallel Cable III Part No. HW-JTAG-PC Software

This cable is not officially supported by Xilinx in any of their recent software releases.  Last point at which it was supported was iMPACT 7.1.  See the following Answer Record

  http://www.xilinx.com/support/answers/8097.htm

 

If you're interested in upgrading, I suggest the HS1 JTAG cable, which is faster and much less expensive ($50) than the Xilinx Platform Cable USB-II ($225).  See info and order the HS1 at

  www.em.avnet.com/jtaghs1

 

Bryan