Reply
Highlighted
New Member
Posts: 1
Registered: ‎03-30-2016

Vita 2000 -> Zync 7000 ->LAN FMC Module

I'm trying to get the VITA 2000 to pass on the pictures or a stream onto the Z702 and then send it out over a FMC LAN connection. This is all just FPGA based without use of the Processor (I dont want to use the Processor, just pure FPGA)

 

So far the Lan Module is implemented and working via UDP based packets sending out Data Frames which are being received on a computer.

 

I'm having trouble with the Vita 2000. With what values can I initialize the camera to start streaming sensor data? What timing should I use?

 

Thank you very much!