Reply
Avnet Employee
Posts: 14
Registered: ‎10-23-2014

Liquid Level sensing, the liquids are oil and YF1234

For and A/C cart for automotive service, customer is looking to measure the liquid level in 3 plastic bottles.

The Cypress kit -022, Liquid Level Sensing works great for water (Er=80). When tried with oil (Er=3) it was ineffective.

Sensing element can be inside the bottle and in contact with the fluid.

 

Does anyone have a suggestion for oil detection? Needs to be about $4 to replace existing solution. (Load Cell)

IR, NFC, proximity???

Resolution needs to be 2mm or better.

Avnet Employee
Posts: 14
Registered: ‎10-23-2014

Re: Liquid Level sensing, the liquids are oil and YF1234

UART interface to the system is preferred.