Reply
Highlighted
New Member
Posts: 1
Registered: ‎07-31-2012

Problems with software load

I can program the fabric on the board (as evidenced by using a GPIO on the LEDs), but neither the esram load or the envm load will work.  

Error in final launch sequence
Failed to execute MI command:
continue
Error message from debugger back end:
Warning:\nCannot insert breakpoint 1.\nCannot access memory at address 0x20000df0\n
Failed to execute MI command:
continue
Error message from debugger back end:
Warning:\nCannot insert breakpoint 1.\nCannot access memory at address 0x20000df0\n
Warning:\nCannot insert breakpoint 1.\nCannot access memory at address 0x20000df0\n

I have extensive experience with Libero/SoftConsole using the SmartFusion (one) for years, but don't understand this one.

Wonder if it is a defect of some type.

Regards

Avnet Employee (Regular Contributor)
Posts: 21
Registered: ‎04-21-2015

Re: Problems with software load

Firstly, are you trying to load the default project from the Support Files and Downloads on the KickStart board page?
Then, are you using SoftConsole 4.0?  This is important, as earlier versions of SoftConsole will not work on the KickStart board because of the FlashPro5 circuitry.