Reply
Regular Contributor
Posts: 23
Registered: ‎05-30-2009

SDTV using EXP module

Hello

 

I would like to operate the tvp5150 on the exp, using microblaze.

I have downloaded "EDK Demos for the Xilinx Spartan-3A DSP 1800A Video Kit" and there is no demo for that.

I can only see the sdtv driver, and it's source code, but i do not understand how to operate it.

Inside xps, i am adding this core from the user ip catalog, and it is added but now what?

 

Regards,

 

Assaf

 

 

Avnet Employee (Star Contributor)
Posts: 471
Registered: ‎04-16-2009

Re: SDTV using EXP module

Assaf,

 

We do not have a reference design for the SDTV interface Iie. TVP5150) on the DRC.

 

Our Asia team created a De-Interlace IP core.

They have a bitstream which showcases this IP core and uses the TVP5150 input.

Contact your local FAE for more information on this design.

 

Regards,

 

Mario.