Reply
Visitor
Posts: 2
Registered: ‎03-17-2010

trace delay for RST_DQS_DIV,sum of DDR ClK and DQS or only matched length to one of them???

Hi guys,

according to MIG documentation and Xilinx Application notes,RST_DQS_DIV trace delay needs to be equal to sum of trace delays of DDR clock and DQS and it's been properly commented in schematic of Spartan3A-DSP.

but in net lenght report of the board layout,total trace length of RST_DQS_DIV is nearly matched to DDR clock/DQS trace and it is not sum of them at all.

e.g total DDR clock (including pre & post series termination) = 3613mils,total DQS trace length = 3813 mils so RST_DQS_DIV needs to be 7426mils approximately but it is only 3794mils.

 

I would appreciate if anybody can clarify this issue for me.

 

Thanks

Avnet Employee (Star Contributor)
Posts: 471
Registered: ‎04-16-2009

Re: trace delay for RST_DQS_DIV,sum of DDR ClK and DQS or only matched length to one of them???

The trace length needs to be the equal to sum of trace delays of DDR clock and DQS, as documented in the schematics.

 

I asked one of our hardware designers to check this trace length on the Rev.C board.

Using the PADS, the tool in which the board was designed, the trace length is 6.9126”.

 

How did you take your measurement ?

For which hardware revision did you make your measurement ?

 

Regards,

 

Mario.

 

Visitor
Posts: 2
Registered: ‎03-17-2010

Re: trace delay for RST_DQS_DIV,sum of DDR ClK and DQS or only matched length to one of them???

Hi Mario,

it is Rev 1 of Spartan 3A DSP starter kit(XtermeDSP).

I looked at net lenght report(which is an excel file) accompanying with Gerber files.you can find it attached.

RST_DQS_DIV=3794mils total

 

CLK_FB_MB=1507.09mils total

 

FPGA_DDR_CLK0_N=3653.79mils total

FPGA_DDR_CLK0_P=3600.87mils total

DDR2_LDQS#_0=3813.58mils total

DDR2_LDQS#_1=3854.64mils total

 

do you think this report has error?maybe daVinic Board has different routing lenghts.

 

Thanks

 

 

 

Highlighted
Avnet Employee (Star Contributor)
Posts: 471
Registered: ‎04-16-2009

Re: trace delay for RST_DQS_DIV,sum of DDR ClK and DQS or only matched length to one of them???

Sorry, I thought you were talking about the Spartan-3ADSP DaVinci co-processing board.

 

I asked one of our hardware designers to check this trace length on the Spartan-3ADSP Starter Kit Rev.1 board.

Using the PADS, the tool in which the board was designed, the trace length is 6.905” (plus the length of the series resistor).

 

Where did the "net length report" excel file come from ?  (I did not see it in attachment)

Did this come from the Avnet DRC web site ?  or the Xilinx web site ?

I will try to find out why it does not have the same information.

 

Regards,

 

Mario.