Reply
Newbie
Posts: 1
Registered: ‎01-24-2014

Connecting with a EXP High-Performance SerDes Module with Easy FPGA Interface

As part of a research project, we are trying to create a hi-speed connection between a TI projector and a PC.  The TI projector can use a EXP High-Performance SerDes Module with Easy FPGA Interface as a daughter board and we want to connect this to a PC through a Spartan 3A.  Wondering if this is even possible and if so, how do you connect the two boards together?

Avnet Employee (Star Contributor)
Posts: 607
Registered: ‎04-20-2009

Re: Connecting with a EXP High-Performance SerDes Module with Easy FPGA Interface

The EXP module is not compatible with the Spartan-3A Evaluation board. It was originally designed to work with the Spartan-3A DSP Starter Kit. Given this setup is 6 years old, you might want to work with your local Avnet FAE to investigate newer options.

 

Bryan