Reply
Visitor
Posts: 6
Registered: ‎05-16-2015

Re: Windows 7 Compatability.

[ Edited ]

for those who read this thread:

I have Win 7 Home Premium with ISE 14.7 and used the Vista driver fpr install. In the device manager it shows up as "Avnet_Sp3A_Demo_XP2_Vista" Port9. So it seems to be installed.

 

Regarding the other question: From my former work with system generator, the tool either requires detailled information about the utilized board or one has to create pcb definition on one own. I tried this for the Spartan 3E PCB at this point of time and failed, allthough I folloed the system generator's spec and docu. For the other board, the Virtex4 Extreme DSP it worked all automatically from the first minute. This board is know to system generator.

 

 

 

 

Highlighted
Visitor
Posts: 6
Registered: ‎05-16-2015

Re: Windows 7 Compatability.