Reply
Visitor
Posts: 1
Registered: ‎04-14-2015

AES-FMC-MC1 on Zedboard

Hey all, 

I recently purchased the AES-FMC-MC1 Motor Control FMC Module, which is listed as Zedboard compatible, however I have been unable to find any tutorials or instructions on how to setup the kit on the Zedboard.

When I try to run the reference design using the Xilinx ChipScope, I receive the error “Error shows in the status register, release done bit is NOT 1,” which I suspect is because the bitsteam is for the Spartan-6, not the Zedboard.

Can anyone please point me in the right direction so I can run the motor kit with my Zedboard.

Thanks in advance!

Avnet Employee (Star Contributor)
Posts: 111
Registered: ‎07-07-2009

Re: AES-FMC-MC1 on Zedboard

Please see the response posted on ZedBoard.org.  Thanks.

 

http://zedboard.org/content/aes-fmc-mc1-motor-control-module-design-zedboard

 

Matt

Visitor
Posts: 1
Registered: ‎10-15-2013

Re: AES-FMC-MC1 on Zedboard

Hello

 

can any body give me the motor specification which can be used with FMC Motor Control card.

 

Any update on this would be of more helpful to me

 

Any weblink from where to get the motors would be great.

 

Regards

Prakash G

Highlighted
Avnet Employee (Star Contributor)
Posts: 111
Registered: ‎07-07-2009

Re: AES-FMC-MC1 on Zedboard

The Hardware User Guide for the module is here -- https://www.em.avnet.com/Support%20And%20Downloads/FMC_MC1_HG_20120821.pdf

Look at sections 2.4 and 2.5.

 

In general the module can drive (2) 3-phase BLDC motors or (1) bi-phase stepper.

The module can deliver 3.5A to each motor, up to 24V when powered through the external power connector.  Otherwise you're limited to a total of 12V @ 1A supplied from the VITA57 FMC connector.

 

/Matt