Reply
Highlighted
Visitor
Posts: 5
Registered: ‎07-19-2013
Accepted Solution

An unknown error

Sir,

       When I am trying to execute this tutorial example link given below: 

http://community.em.avnet.com/avnet/attachments/avnet/Spartan-6LX150T/266/1/S6-LX150T%20-%20Hardware...

 

I am getting an error like " An unknown error was encountered while compiling the design for hardware cosimulation " while I am trying to generate the point to point ethernet cosimulation block...

What can be the reason  ???

 

Visitor
Posts: 5
Registered: ‎07-19-2013

Re: An unknown error

sir,


The problem got solved...the main problem lies with the example model provided in the Xilinx 14.x version...I have searched one more version of the model developed in ise 13.2...updated it in 14.x sysgen environment and then executed...its running fine..
thanks
 
 
Best Chandrajit