Reply
Visitor
Posts: 5
Registered: ‎07-19-2013
Accepted Solution

Avnet Spartan 6 IVK, pin location and boundary scan position information needed

 
Sir,
I am going to process an image using the Avnet Spartan 6 Industrial video processing kit(by JTAG cosimulation)..(family, part, speed, package) has been shown in the figure below...but couldn't find out the pin location and the boundary scan position..Can you pls mention it...Is the clock frequency correct(100 MHz) as 
  • On-board 100MHz LVTTL oscillator has been mentioned..

 Pls see the attached file for your reference...

 

ERROR.bmp
Avnet Employee (Star Contributor)
Posts: 471
Registered: ‎04-16-2009

Re: Avnet Spartan 6 IVK, pin location and boundary scan position information needed

System Clock

   Frequency : 100 MHz

   Pin : U23

 

JTAG Options

   Boundary Scan Position : 3

   IR Lengths : 16, 16, 16

 

Regards,

 

Mario.

  

Visitor
Posts: 5
Registered: ‎07-19-2013

Re: Avnet Spartan 6 IVK, pin location and boundary scan position information needed

Thanks sir for the reply...but the IR length will be 16,16, 6 as it has shown in the device when  detected ...

Avnet Employee (Star Contributor)
Posts: 471
Registered: ‎04-16-2009

Re: Avnet Spartan 6 IVK, pin location and boundary scan position information needed

You are correct, good catch !

 

System Clock

   Frequency : 100 MHz

   Pin : U23

 

JTAG Options

   Boundary Scan Position : 3

   IR Lengths : 16, 16, 6

 

Regards,

 

Mario.