Reply
Regular Visitor
Posts: 2
Registered: ‎02-07-2011

Base Platform Demo Issues

[ Edited ]

Hello,

 

I try to tested Base Platform design which base on EDK13.2.

Also, i have two FMC board that FMC-IMAGEOV and FMC-DVI.

When i testing IVK + FMC board then i can see "No FMC module detected" message on my serial terminal.

----------------------------------------------------------------------------------------

Terminal message so on....

No FMC module detected
If there is no FMC module, the output of FMC Module Validation code will be:
FMC Module Validation
[fmc_ipmi_get_common_info] FRU_I2C_ERROR (idx=0)
ERROR : No FMC module detected

----------------------------------------------------------------------------------------


I checked up IIC signal on FMC board and there was no problem as i see.

 

And, i traced S/W function which return wrong value(retval /= FRU_SUCCESS).

 

So, i guessed that EEPROM data currupted by some conditions.

 

Can you provide this IPMI EEPROM image file?

 

If yes, how can i re-program?

 

Thanks,

Anderson

 

 

Avnet Employee (Star Contributor)
Posts: 471
Registered: ‎04-16-2009

Re: Base Platform Demo Issues

Please use the following factory test designs to re-program the FMC's identification EEPROM.

 

FMC-IMAGEOV (populated on FMC slot FX1):

   File name: FMC_IMAGEOV_factory_test_suite_20100721.zip
   Website link: https://avnet.egnyte.com/h-s/20110930/29faabb231664b0c

   Run the I2C test in the following sub-directory:

      FMC_IMAGEOV_factory_test_suite_v1\I2C\s6ivk_i2c\s6ivk_fmc_imageov_i2c_test.bat

 

 

FMC-DVI (populated on FMC slot FX2):

   File name: FMC_DVI_factory_test_suite_20100720.zip
   Website link: https://avnet.egnyte.com/h-s/20110930/5891f966cc7d4a49

   Run the I2C test in the following sub-directory:

      FMC_DVI_factory_test_suite\I2C\s6ivk_i2c\s6ivk_fmc_dvi_i2c_test.bat

 

The factory test designs use the DB9 connector (P3) for the serial port.

A serial terminal (9600baud) is needed to specify the serial number of the board. 

Type the serial number indicated on the sticker then press enter.

 

Regards,

 

Mario.

Highlighted
Regular Visitor
Posts: 2
Registered: ‎02-07-2011

Re: Base Platform Demo Issues

Hi Mario.

 

I'll try to your answer.

Thank you

 

Regards,
Anderson.