Reply
Highlighted
Regular Visitor
Posts: 9
Registered: ‎06-24-2010
Accepted Solution

OV9715 module

Hi all,

We need to add a second OV9715 sensor module to

the IVK board in order to implement a stereovision algorithm.

I've searched the Avnet site but I haven't found that module.

 

Does anyone know if it is possible to buy a preassembled sensor

 module such as the one included in the IVK kit?

 

Regards,

Giovanni

 

 

 

 

Avnet Employee (Star Contributor)
Posts: 471
Registered: ‎04-16-2009

Re: OV9715 module

Giovanni,

 

The OV9715 image sensor can be purchased from Avnet:

   AES-ACC-OV9517-G (camera and ribbon cable)

 

Regards,

 

Mario.

Contributor
Posts: 12
Registered: ‎02-14-2011

Re: OV9715 module

Hi,

 

I am purchasing the OV9715 module separately from the IVK, and was wondering if there are any datasheet or documents available for it ? 

 

Thanks

Avnet Employee (Star Contributor)
Posts: 471
Registered: ‎04-16-2009

Re: OV9715 module

The OV9715 image sensor module comes with a CD containing the following:

- Application Notes :

   - EAAA Prototyping Module Quick Start Guide, v1.0

   - OmniVision Serial Camera Control Bus (SCCB) Functional Specification, v2.2

- Technical Bulletin :

   - OmniVision Assembly Guidelines, v1.1

 

The datasheet for the OV9715 image sensor must be requested at:

The datasheet request process includes the signing of an NDA with OmniVision.
 
Regards,
 
Mario.