Reply
Visitor
Posts: 1
Registered: ‎01-12-2014

VDMA Reference design

Hello community,

 

I have purchased a spartan6 video development kit, and I want to simple working VDMA reference design. Is there any?

 

I have developed an IP core that can generate a timing + test pattern, when it's directly connected to an HDMI controller, I can see the video as expected.

 

I'm trying to make use of Xilinx VDMA in a microblaze environment.

 

MY IP > v_vid_in_axi4s > VDMA > v_axi4s_vid_out > HDMI

                     \_______ timing_______/^

 

What's the proper VDMA paramters? Should I use FSYNC=0/1/3? What FLUSH should be set?

 

My IP generates a 60fps vide,  the write channel works at lower rate (~10fps), the write channel gets many errors:

EOLLate - SOFLate - EOLEarly - SOFEarly - DMAInt

 

How can I debug this?

 

Any tip is appreciated.

Thanks

 

Highlighted
Avnet Employee (Star Contributor)
Posts: 471
Registered: ‎04-16-2009

Re: VDMA Reference design

The first place to look is the product page:

http://www.em.avnet.com/en-us/design/drc/Pages/Xilinx-Spartan-6-FPGA-Industrial-Video-Processing-Kit...

 

Click on Support File & Downloads to access the download page:

The "EDK Designs - DVI/Camera Video Processing and Frame Buffer"  link contains the frame buffer design examples.

 

-------------------------------------------------------------------------------------------

 

There are no designs for the Spartan-6 Video Imaging and Processing Kit that make use of the AXI4-Stream adapter cores.

 

Take a look at the following product page:

http://www.em.avnet.com/fmc-imageon 

 

In the downloads section, there is a "Creating a Video Design from Scratch" tutorial, which describes how to configure the AXI4-Stream adapter cores, as well as the AXI_VDMA core.

 

Although this tutorial does not target the same hardware that you have, it will provide usefull information about the video cores.

 

Regards,

 

Mario.