Reply
Contributor
Posts: 10
Registered: ‎11-27-2013
Accepted Solution

Is it possible to perform video compression (h.264) using Spartan-6 LX 150T development kit?

 
Avnet Employee (Star Contributor)
Posts: 511
Registered: ‎05-05-2009

Re: Is it possible to perform video compression (h.264) using Spartan-6 LX 150T development kit?

Please provide more info on how you are planning on using the LX150T board.

Contributor
Posts: 10
Registered: ‎11-27-2013

Re: Is it possible to perform video compression (h.264) using Spartan-6 LX 150T development kit?

Using matlab-simulink. I am planing to convert the simlink model to hdl using system generator.

Avnet Employee (Star Contributor)
Posts: 471
Registered: ‎04-16-2009

Re: Is it possible to perform video compression (h.264) using Spartan-6 LX 150T development kit?

[ Edited ]

Yes, it is possible to perform video compression on the Spartan-6 LX150T development kit.

 

H264 IP is available from the Xilinx ecosystem of third party IP vendors.

 

Please consult the following Xilinx web page for more information:

                http://www.xilinx.com/publications/prod_mktg/smarter-vision-ip-reference-designs.htm#encoding

 

One of the partners listed as supporting H264 on Spartan-6 is CoreEL:

 

CoreEL

                http://coreel.com/pages/productsDigitalVideoH264IframeCodec.aspx

 

 

Jointwave also provides H264 IP and has a demo available for the Spartan6-LX150T board (requires FMC-DVI module):

 

Jointwave

                http://www.jointwave.com/demos.html

                http://www.jointwave.com/userdocs/Jointwave%20H.264%20Encoder%20Live%20Demo%20User%20Guide%20-%20Xil...

 

Regards,

 

Mario.

Highlighted
Contributor
Posts: 10
Registered: ‎11-27-2013

Re: Is it possible to perform video compression (h.264) using Spartan-6 LX 150T development kit?

Thanks AlbertaBeef,

 

But those H264 IPs are two costly. I already talked with coreel and A2e Technologies