Reply
Contributor
Posts: 10
Registered: ‎11-27-2013

Is it possible to work with Network cameras using spartan-6 industrial ethernet kit??

Soon i will get spartan-6 industrial ethenet kit ( Spartan-6 LX150T Board) and samsung network camera (PTZ Domes-SNP-3120VH). Is it possible to work with this camera?

 I want to take the video i/p from this camera and i have to compress it. I already done with the coding now i am not getting whether this camera will work or not?

 for camera specifications refer the below link:

https://www.samsung-security.com/products/security-cameras/network-cameras/ptz-domes/SNP-3120VH.aspx

--
Thanks

 

Hemanth K

Avnet Employee (Star Contributor)
Posts: 511
Registered: ‎05-05-2009

Re: Is it possible to work with Network cameras using spartan-6 industrial ethernet kit??

If the camera interface to board is Ethernet, I don't see any reason why it would not work.

Contributor
Posts: 10
Registered: ‎11-27-2013

Re: Is it possible to work with Network cameras using spartan-6 industrial ethernet kit??

THANKS,

 

Do i need to develop any ethernet core or i can simply connect it to the kit  and adding input loc  in the code?