Reply
Contributor
Posts: 10
Registered: ‎11-27-2013

Will USB Camera works with Spartan-6 LXT150T development kit?

I have an USB Camera and I will get  Spartan-6 LXT 150T board soon. I am planning to perform h.264 video compression using USB camera. Will it work  or do i have to purchace any other camera?

Avnet Employee (Star Contributor)
Posts: 511
Registered: ‎05-05-2009

Re: Will USB Camera works with Spartan-6 LXT150T development kit?

You would need a USB Host IP core and a USB host adater cable.

Contributor
Posts: 10
Registered: ‎11-27-2013

Re: Will USB Camera works with Spartan-6 LXT150T development kit?

What is the use of usb host adapter cable? i think usb port is available In spartan-6 lxt150t board such that directly i can connect my usb camera to the board.

 

will USB host ip core is freely available or do i have to purchase?

Avnet Employee (Star Contributor)
Posts: 511
Registered: ‎05-05-2009

Re: Will USB Camera works with Spartan-6 LXT150T development kit?

If your camera can directly connect to the USB connector on the board, then you would not need the adapter. I'm not aware of any free USB host IP cores.