Reply
Newbie
Posts: 1
Registered: ‎03-21-2014

errors with pin assignment H25 for sys_reset_n (AXI PCIe Endpoint Design)

I try to generate a bit file for using the PCE Endpoint. If I follow the instructions written down in the Avnet S6LX150T Development Board AXI PCIe Endpoint Design (version 1.0) June 2011 then I get errors.

The reset pin H25 should be incorrect..

Page 17 describe:

modify the .....ucf file and assign pin H25 to the sys_reset_n signal. Save and close the UCF.

Done that but with errors as a result..

 

Avnet Employee (Star Contributor)
Posts: 511
Registered: ‎05-05-2009

Re: errors with pin assignment H25 for sys_reset_n (AXI PCIe Endpoint Design)

Unfortunately, that's an error in the documentation. The PCIe reset signal should be assigned to pin V20.