Reply
Visitor
Posts: 5
Registered: ‎07-19-2013

avnet spartan 6 IVK pin location and the boundary scan position information needed

Sir,
         I am going to process an image using the Avnet Spartan 6 Industrial video processing kit(by JTAG cosimulation)..(family, part, speed, package) has been shown in the figure below...but couldn't find out the pin location and the boundary scan position..Can you pls mention it...Is the clock frequency correct(100 MHz) as 
  • On-board 100MHz LVTTL oscillatorhas been mentioned..

 

Inline image 1

Highlighted
Avnet Employee (Star Contributor)
Posts: 471
Registered: ‎04-16-2009

Re: avnet spartan 6 IVK pin location and the boundary scan position information needed

This question was answerred on the Spartan-6 Industrial Video Kit forum:

   http://community.em.avnet.com/t5/Spartan-6-Industrial-Video-Kit/Avnet-Spartan-6-IVK-pin-location-and...