Reply
Avnet Employee
Posts: 6
Registered: ‎05-17-2011

FMC 150 with Spartan LX75T board from Avnet

Hi ,

 

I have Avnet LX75T developement kit from Avnet. I want to use FMC 150 card with LX75T board.

 

Is there anybody who has tested FMC 150 with LX75T.

Avnet Employee (Super Contributor)
Posts: 79
Registered: ‎04-17-2009

Re: FMC 150 with Spartan LX75T board from Avnet

Although I have not tested the FMC150 module with the S6LX75T board, I would expect this FMC card to work with this board.  Both the FMC150 and S6LX75T are designed with a 2.5V I/O FMC interface.

 

--Tom

 

--
Tom Curran