Reply
Visitor
Posts: 1
Registered: ‎10-17-2012

IVK libraries for S6LX75T

I have S6LX75T development board and FMC image OV card with dual omni camera.

I mentioned that SP605 video kit have IVK libraries to demonstrate the FMC image OV card to display camera captured images.

 

Can't I use or modify this IVK libraries for S6LX75T board ?

 

Best regards,

Fadjar

 

Highlighted
Avnet Employee (Star Contributor)
Posts: 471
Registered: ‎04-16-2009

Re: IVK libraries for S6LX75T

Jadjar,

 

The S6-LX150T based reference designs contain pcores that are targetted for the Spartan-6.

These pcores can be used for the S6-LX75T board.

 

I do not have a design for the S6-LX75T + FMC-IMAGEOV hardware combination ready off the self.

 

You will have to modify the UCF file for the new pin locations.

There may also be changes related to the main on-board oscillator, and the on-board I2C chain.

 

Regards,

 

Mario.