Reply
Newbie
Posts: 1
Registered: ‎12-16-2013

Linux driver for LX75T PCIe Dev Kit

Is there a linux driver available for this kit or any information about using this board in a linux environment.

 

Thanks

Visitor
Posts: 2
Registered: ‎01-07-2014

Re: Linux driver for LX75T PCIe Dev Kit

I've installed this card in my linux box and verified it works. No driver need. Running Fedora 14. There is no linux driver for the Avnet PCIe Demo software.  But, if you follow the instructions in the "Programmed I/O Example Design" (found HERE), you can verify it works by obtaining a small program called "pcimem".  Get pcimem HERE and follow the app's help to get it to work. It maps PCI memory to user application memory and you can write to registers directly with it, and hence toggle LEDs/read DIP switch positions which is what the PIO Example Design by Avent provides.