Reply
Regular Visitor
Posts: 3
Registered: ‎07-30-2012

Spartan-6 LX75T Kit is not shown as Co-processor with Avnet nano-ITX mother board

After following each step as in Lab exercise 2 and 3 given with the board, I am not able see the Spartan 6 PCIe board as coprocessor. When i am running the Avnet PCIe demo, it is saying invalid parameter.

Kindly help me to sort out this issue.

 

thanks 

Vaibhawa 

 

PS: I have follow each step very carefully. 

Avnet Employee (Super Contributor)
Posts: 79
Registered: ‎04-17-2009

Re: Spartan-6 LX75T Kit is not shown as Co-processor with Avnet nano-ITX mother board

The 'invalid paramter' error indicates the software driver is not installed or is not loaded by the OS.  What version of Windows are you using?  32-bit or 64-bit?

 

--
Tom Curran
Regular Visitor
Posts: 3
Registered: ‎07-30-2012

Re: Spartan-6 LX75T Kit is not shown as Co-processor with Avnet nano-ITX mother board

I have installed Windows Embedded Standard  7 ( 32-bit) service pack 1. Let me know how to include the driver for PCIe. One thing i nedd to share that i have installed Chipset driver that include PCI drivers also. Can u send me the source file of PCIe demo application.

 

 

 Thanks 

Vaibhawa