Reply
Visitor
Posts: 1
Registered: ‎04-20-2016

Question on Microblaze in LX9 MicroBoard

Good morning.

 

I'm using "Spartan 6 LX9 Microboard, MicroBlaze " dev. board for the first time.

I need to know if it's possible to make a preliminary backup and storing Microblaze. I desired to program the FPGA (Spatan-6) with Xilinx ISE, but I don't want to lose data. I want also restore Microblaze and using web application.

Avnet Employee (Star Contributor)
Posts: 613
Registered: ‎04-20-2009

Re: Question on Microblaze in LX9 MicroBoard

The Spartan-6 itself is SRAM-based and therefore, volatile. Anything that you want preserved must be stored off-chip in a non-volatile resource. One such resource is the on-board QSPI Flash.

Bryan